I'm working on a bq78PL114 EVM. I'm simulating cells using resistors as shown in the user guide. Without being hooked up to the board, I see 3.6 V across each "cell." But after hooking them up to the board, the fault LED comes on and the resistors don't have the same voltage across them. Of the six, the first four measure 4.1 V and the last two measure 2.5 V. I saw the warning in section 4.1 about PowerPump currents causing voltage fluctuations. Could this be the problem? What can I do to resolve this?
Thanks,
Ronald Deang