Hi, my name is Loc Ngo, an electrical designer of high voltage DC-DC at ABB Plano Texas. I am using LM5021 for my small bias power to convert 360V-400V to 12V in primary side and 12V for secondary side, currents for each side approximately 100mA of each. Switching frequency is 500Khz, transformer turn ratio is 33/5/5 and total inductance is 425uH. I am getting cycle skipping and operating duty cycle is just 2% at Vin of 360V, already tried to add the offset voltage to the current sense pin but still not help, cycle still skipping.
Would you please help to resolve this issue?
my email address is loc.ngo@us.abb.com
Thanks
Loc