This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: Battery is not charging completely

Part Number: BQ25606

Hello,

I have the board with schematic built as below. All the output voltages seem to be working. The resistor around ILIM is 415 Ohms and resistor for ICHG is set to 1.051k Ohms. 

Now I have set the charging current on power supply as 1.1A at 5V and I provide input to the VUSB directly. 

I see that the status led is on and battery is charging at 300mA current. I even notice the voltage at battery is increasing from 3V - 4.2V. Eventually IC went into voltage regulation mode.

In my case the charger never reached ICHG current which was set to 600mA current approx.

Am I missing something here? Why is the charge current not reaching 600mA.

Any input would be helpful.

Thank you.