This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power IC for operating Laser Driver



We are looking for the IC and circuit information.

Input voltage : 3.3V 

                        3.3V inputs the IC by square wave 500nS pulse.

Output voltage : -5V

Output current : 1.5A(max)

We need -5V to operate Laser Driver.

Please tell us the recommended IC and circuit.

We are concerned that input voltage(3.3V) is very short pulse(square wave 500nS).

Best regards,

Takahiro Nishizawa

  • Thank you for your support!

    How is your situation?

    We hope your earlier answer.

    Best regards,

    Takahiro Nishizawa

  • Hi Nishizawa-san,

    What sort of power IC are you looking for? I would assume that since you have a positive input voltage and need a negative output voltage for the laser driver that you are looking for a switching regulator to do that conversion. Is this what you have in mind?

  • Hi Takahiro Nishizawa,

    1.Is this power for EML bias or PD laser driver ? could you please share the partial block diagram ?

    2. why your input voltage is square wave? is this has a capability to supply -5V/1.5A output ?

    3. Do you want a continuous -5v output or a square -5V wave?

    Best Regards,

    Kevin

    If this answers your question, Please click "This resolved my issue" button.
    ____________________________________________
    TPS62810-Q1 – New Automotive 6Vin, 2.25MHz buck family with 1% accuracy and SYNC-pin. 1-2-3-4A options.
    Smallest 2x3QFN package with wettable-flanks for optical PCB inspection.

  • Hi Takahiro Nishizawa,

    Since I have not received your reply for several days, I will turn off this item. If you have further question, you can reply it again.

    Best Regards,

    Kevin

    If this answers your question, Please click "This resolved my issue" button.
    ____________________________________________
    TPS62810-Q1 – New Automotive 6Vin, 2.25MHz buck family with 1% accuracy and SYNC-pin. 1-2-3-4A options.
    Smallest 2x3QFN package with wettable-flanks for optical PCB inspection.