Other Parts Discussed in Thread: TPS2490
Dear Specialists,
My customer is considering TPS2491 and has a question.
I would be grateful if you could advise.
---
I am considering MOSFET of TPS2491.
The datasheet P.21 says, "A VGS rating of ±20 V is required, because the TPS2490 can pull up the gate as high as 16 V above source."
I think this reason GATE output voltage of TPS2491 can be 16Vmax.
Regarding negative voltage, it doesn't need to consider.
The reason of +/-20V, the rated voltage of VGS often has the same value for positive voltage and negative voltage.
So it can use MOSFET VGS(+20V/-12V), is it correct?
---
I appreciate your great help in advance.
Best regards,
Shinichi
日本金銭機械株式会社 第1研究開発本部 製品開発部 製品開発2グループ
明石様
いつもお世話になっております。
富士エレクトロニクスの井上です。