Hi,
I have a question about TPS65941.
I checked I/O levels of PMIC, and the GPIO11 of PMIC-A is pulled up to VDA_MCU_1V8 in EVM schematic. (GPIO4 of PMIC-B is also pulled up to VDDR_BIAS_1V1)
Is it correct? The output pin type of GPIO4(IO level is 1.8V) and 11(IO level is 3.3V) is push-pull, so I think this pin doesn't need to be pulled up.
Could you please give me a comment?
Thanks,
Manwoo Kim