Part Number: LM3481
Other Parts Discussed in Thread: LM5155
Hello,
I am designing a SEPIC converter with input voltage ranging between 9 and 100 VDC. The output shall be fixed at 48 VDC. Current load on output is up to 2A.
My question is if I can use the LM3481 with a separate 12V supply to the Vin pin (since the maximum voltage of the LM3148 is 48V), and then connect the 9-100V supply to the inductor/MOSFET on the outside? I,e he Vin pin will be separated from the 9-100 V.
I guess the question comes down to if the Vin voltage is used as a reference for the regulation inside the chip, or if it is just used for logic and MOSFET driver supply.
Thanks in advance.
Lars