This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: tl431

Part Number: TL431

Hi 

I am using TL431 for over voltage protection in my LED Driver. TL431 is used to pull down the VCC of my controller (FL7733-Fairchild). In some cases, TL431 got damaged in Surge Testing. I tried to address the issue, but it do not create any results.

LED Driver details 

Input Voltage : 100VAc to 300VAC

Power : 24W

Over Voltage Cutoff - 325VAC

IC VCC- 22V Maximum

Note : Failure is occurred rarely. TL431's Cathode and Anode getting short.