Hello
I need to design a dcdc power supply with mainly four operation modes:
1. Vin 48V -> Vout 24V
2. Vin 48V -> Vout 24V..12V (adjustable)
3. Vin 24V -> Vout 24V
4. Vin 24V -> Vout 24V..12V (adjustable)
In all modes Iout ranges from 50mA to 2A.
I have no problem with the 48V operation and the adjustable output. (TPS54260)
Can you propose me the buck chip which can produce an outputvoltage as close as possible to the input voltage?
The aim is to produce an output voltage as close as possible to the 24V input.
Is there a design where I can switch the input directly to the output without regulation?
Thanks, greets Marc