hi Team:
1. If only D+.D- is connected together and not connected to the D+,D- of USB, is the input current limited to 3A?
2. I have connected D+,D-with USB D+,D-,The schematic diagram is shown below! USE 5V to 2S bat charge!
When BQ25886 first input, 5V power supply , then inserted the battery . The charging current is 950mA.
When first inserted the battery then the 5V power is added to the BQ25886, and the charging current is 640mA?
Why are there different charging currents?