Hi
We want to use BTP Function as external interrupt out put for SOC Low Level indicator.
But this BTP has 2 status condition.
• OperationStatus()[BTP_INT] is set when:
– Current > 0 and RemCap > “clear” threshold (“charge set threshold”). This threshold is initialized at
reset from Settings.BTP.Init Charge Set.
– Current ≤ 0 and RemCap < “set” threshold (“discharge set threshold”). This threshold is initialized at
reset from Settings.BTP.Init Discharge Set.
But we want to use just under remap threshold for interrupt status.
[ Question ]
1) Dose we use just under Remcap threshold status ??
For instance
BTP Level Hi -- > Low when Remcap under threshold level.
Yes , BTP has 2 function , Host side dose not judgement these 2 condition.
RemCap > “clear” threshold
RemCap < “set” threshold
Can we possible Disable RemCap > “clear” threshold condition ??
2) Could you tell us BTP Pin electrical spec ??
For instance 3.3V or 1.8V output ??
Regard
March Jasper ( Disty Sugimoto )