Dear TI,
We found the following problem in the FLY BACK circuit configured by applying LM5180-Q1.
(Three identical circuits are configured on the board.)
- Problem: Abnormal operation occurs when power on / off.
> In case of ch3, when input 12V off, output voltage 15V rises to about 18V and then falls.
> In case of ch2, when input power is on, it rises to about 17V and then stabilizes at 15V.
I would like to request a cause analysis of this issue.
Please review and let us have your feedback soon.
Thank you.