Part Number: BQ24133
Other Parts Discussed in Thread: BQ24171, BQ24172
Hi Team,
Could you help on this request:
We need to load a battery pack formed by two cells in series, the supplier recommends a charge voltage of 4V / max 4.1V per cell, while I understand that the BQ24133 has a fixed voltage of 4.2V per cell.
Is there any way to adjust this value to lower it as recommended by the battery supplier?
Assuming to load the pack at 4.2V / cell the output voltage must reach 8.4V on the two cells in series.
What is the minimum voltage to which I must supply the BQ (minimum PVCC) for the correct operation of the charger in this condition (max. 1A charge current)?
Regards,
Fabio