Hi, TI member,
We are surveying for TI/TPS25200DRVR and have below question.
Would you mind to help us for below question?
1. Could TI/TPS25200DRVR use for Vin/Vo:3.3V and Vin/Vo:5V?
2.If
Vin=3.3V, Vout=3.3V?
Vin=5V, Vout=5V?
3.If it happens over current/voltage/temperature, TI/TPS25200DRVR will cutoff Vout and output signal.
Is my description correct?
4.Is the threshold of over voltage fixed?
(1)If Vin=3.3V, how is the threshold of over voltage?
(2)If Vin=5V,how is the threshold of over voltage?
5.Is the current limit setting method the same of Vin/Vout:3.3V and Vin/Vout:5V?6.Is the current limit setting
6.Is the current limit setting be below equation?(RILIM)
Thank you.