Hi,
Are there any load behaviour requirements to get accurate ACC or SOH values?
I am thinking of "initial measurements" during "Startup Phase":
Is it ok if the battery is loaded during Startup Phase?
Is it ok if the battery load differs during a Startup Phase?
Is it ok if the battery load differs between different Startup Phases?
Must the battery be in any specific condition (5 hours relaxed, not loaded, etc) when the Startup Phase begins (GE set high)?
I also consider "Update Discharge/Voltage" during Active Phase":
Must the load be constant during an Active Phase?
How will short load pulses (0.5A / 1ms) affect ACC and SOH?
Regards
CHA