Other Parts Discussed in Thread: BQSTUDIO, , EV2400
I saw the description in the datasheet "The value of the current sense resistor should be entered into both CC Gain and CC Delta parameters in the Data Flash Calibration section of the Evaluation Software."
And the range of CC GAIN is from "min 1.00E-01" to "min 1.00E-01", CC Delta is from "min 1.00E-01" to "max 1.19E+06"
What do the registers mean? How to create the relationship between the registers and the sense resistor?
For example, if it is connected to a 20mΩ resistor, how do I configure registers to match?
Thanks.