Sir/Madam,
I am using a BQ25606 in a design and I am having some issues. My application is I am using a single cell 3.6V lipo battery, (5400mAH 26650), to power 5V boost regulator that powers a circuit that draws ~1.8A at 5Vdc. My questions is how much current can be drawn from the battery, through the BQ25606? So can the BQ25606 allow 3A at 3V roughly? I have looked through the datasheet but have been unsuccessful in finding this info?
Thank you in advance.
Scott