Part Number: BQ24630EVM
Other Parts Discussed in Thread: BQ24630
Hello.
I'm using the BQ24630EVM to evaluate the BQ24630 for a battery pack of 6s LiPO4 batteries.
I've changed R7 to 22k to limit adapter current to 3A, R12 to 14k to set charge current to ~2.1A, and R25 to 976k to set charge voltage to ~19.3V.
I'm supplying 24V to ACin. ISET1 testpoint is 0.429v, ISET2 testpoint is 0.299V, and ACSET testpoint is 0.594V as expected
Power switching from Vbatt to ACin works fine, Bat/ACdrv LEDs indicate correctly, PG and CE LEDs indicate correctly, but charging does not occur with batteries depleted to 14.8V.
I've probed test points and TP13 (VFB) is always the same as VCC. Is this a problem with the chip? I assumed VFB is always to be 1.8V on the BQ24630.