This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92602EVM: TPS92602 Evaluation Module

Part Number: TPS92602EVM


Hi ,

One of my customer using TPS92602 Evaluation Module  for LED driver .

In this design there are two output of 75V1A.

Customer need to drive  38 V @ 400 mA  at output channel_1 and 

22V @ 400 mA at Output  channel_2 of  TPS92602BQPWPRQ1.

Please advise what need to be change in this design for achieve required Specification

 

Thanks

Regards

rahul