Other Parts Discussed in Thread: BQ79606EVM-897,
Hello,
For a research project I've got two eval boards (BQ79606EVM-897). I also got the sample code for code composer studio.
I have an Arduino Mega as host to read the registers of the BQ79606A-Q1.
The jumpers of the first eval board are configured as base device, the second one as a stack device.
I copied parts of the sample code and I am able now to read and write registers of the base device (see code below).
My problem is, I cannot establish a connection to the second eval board.
Already during the Auto-Addressing I cannot read back the address of the second board.
How can I debug the daisychain connection between the two boards? Am I missing something to properly write/read from the second board?
Result:
Prog Start
Board 0=00
Board 1=ff
Addressing done
Thank you for your support and regards,
Valentin