Folks,
I'm figuring out how to design a boost converter with low levels of noise. I've read this TI app note about reducing EMI from TPS61088 .
I've also read this Microchip app note (AN1466), which suggests to slow down the turn-on of the integrated MOSFET. This is a fairly common technique, and it's usually implemented by adding a small resistance in series with a MOSFET gate. This is easy to do if one has a controller with an external MOSFET. But what to do with converter ICs which have an integrated MOSFET? The microchip app note suggests to add a resistor in front of the power supply pin which powers the gate driver.
my question: Would a resistor in series with the BOOT pin on the TPS61089 be a viable way of reducing EMI?
The value of the resistor I have in mind is between 10Ω and 100Ω .
Any suggestion, insight or reference is really appreciated!
Cheers,
- Nick