I'm using a BQ40Z50-R2 battery fuel gauge, and while the system seems to be working properly, we are seeing an issue where 2 of the 4 LEDs are a little dimmer on some of our assemblies. I am seeing LEDs 1 and 3 at the same intensity, and then 2 and 4 are at the same intensity. If I swap LED pairs (so the bright two are replaced with the dimmer two), the bright two are now dimmer and vice versa. I think it's related to how you can drive 5 LEDs, and I'm only using 4.
However, this is not happening on all of the BQ40Z50-R2 ICs, but when it does happen, it's repeatable and I can't seem to fix the issue without swapping out the BQ40Z50-R2 for another one. I have this configured just like the example image in the data sheet (figure 35), except LED5 is not present.
Has anyone else encountered this? Is there a fix for this?