This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Fsw waveform of the TPS65400 on the board under investigation is as shown in the attached waveform.
Duty is not constant. Is this operation normal?
A 2A output block is used, but the load is light.
Hi, Sir
1. Is loading changing when you probe the waveforms? (Suggest to probe the waveforms at constant loading.)
2. Could you send me schematic for reviewing?