Other Parts Discussed in Thread: UCC21222, UCC21540, UCC21220, UCC21520
Dear TI Experts,
Could you please suggest a best suitable Isolated gate driver from TI?. Which should have the following features.
1. Should be isolated driver
2. Should able to drive the high side
3. Should able to with stand a DC link voltage of 500V
4. Should be fast enough of driving 400V input to 60V/20A output full bridge MOSFETS.
Regards
Aneesh