Other Parts Discussed in Thread: TPS717
Folks,
I’m reading the datasheet for the TPS65721 (linear charger with buck converter and LDO). Fig. 23 shows a typical application towards a Bluetooth power supply. The TPS65721 generates the +1.85V supply rail for Bluetooth in two stages: buck, then LDO.
The buck is witching at 2.25 MHz. Does the LDO have an appreciable PSRR at 2.25 MHz? Power supply rejection of a good LDO (like TPS717) is only up to about 1 MHz.
my question: What’s the merit of following a high frequency buck with an LDO?
Any suggestion, insight or reference is really appreciated!
Cheers,
- Nick