This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC-DC Buck converter latest Reference design

Hi,

I would like to design 2 x separate DC-DC buck converters (3.3 VDC and 5 VDC outputs) that meet the specification given below:

Vin Range = 8 VDC - 30 VDC, Iout = minimum of 500 mA - 1 A (I do not mind higher output current but want to keep the size of the design compact).

I was wondering if there is a new part and application note that you would recommend that also tackles/advise on the EMC / CE / RE related issues. Your guidance will be much appreciated.

  • Hi Inno,

       About new part, it is better for you to use Webench to design.

      About apps note, I recommend the following:

    •Texas Instruments, There are more ways than you think to reduce conducted EMI, Blog

    • Texas Instruments, Automotive EMI Reduction Techniques, Applications and Solutions, Training Video

    • Texas Instruments, Understanding EMI and Mitigating Noise in DC/DC Converters, Training Video

    • Texas Instruments, Simple Success With Conducted EMI From DC-DC Converters, (SNVA489)

     

    Gavin