Other Parts Discussed in Thread: BQSTUDIO
Hi,
1). i want to config the bq34z100-g1,please help check the following parameters, thanks;
the battery(5p6s) information:max voltage-->25.5V rated voltage:22.2V max capacity:28.5AH
my settings:
Design capacity:9500mAh
Design energy:21090mWh
Design energy scale:10
current calibration scale:3(load 6A,calibrate to 2A)
2) .i was following the detailed design procedure in the BQ34z100-g1 datasheet(Page50) http://www.ti.com/lit/ds/symlink/bq34z100-g1.pdf ;at the step 4,i was failed to change the CC Delta;my Rsense is 1mOhm;after voltage calibration,the CC Delta and CC Gain become 10.184;when i changed these two registors to 1mOhm,the CC Gain was OK,but CC Delta kept the value unchanged ;