Other Parts Discussed in Thread: BQ30Z55, GPCRB
Hi TI
Bq30z55 low temperature log as attached
Capacity can be released, but RSOC only shows 2%
It's normal at room temperature.
How to solve it?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI
Bq30z55 low temperature log as attached
Capacity can be released, but RSOC only shows 2%
It's normal at room temperature.
How to solve it?
Thank you
Hi Batt
Thank you very much.
You mentioned three modification values. Which one is more likely to be 0 or 1 or 3?
In the GG file of the problem battery, it is found that there are more than two values of - 900 in the RA table. Is there any problem?
If so, what are the possible causes?
Regards,
Jerry
Hi Jerry,
Please use 1 or 3. I can't really say if the Ra values are a problem unless I see the battery log and previous Ra value.