Other Parts Discussed in Thread: BQ76940, , BQSTUDIO
LIke the title says:
My 12S1P 32000mAh lipo battery work with BQ78350-R1 + BQ76940 power ICs, everything works well except the cycle count somtimes jumped to 5911 which actually is 5- 10times.
Now i have 40 batteries, all used below 10 times and the cycle count of 6 have jumped to 5911, and if you continue to use it, it will be still 5911 and never change again.
Battery usually works at current about 30-45A, and the charge current is 40A,.
Its works on a drone, and the designed max discharge current is 150A,actually we dont use mosfet because we dont think its safe enough to shut the ouput off when something wrong happens.
Now just the cycle count of 5911, we cant solve it , and dont why , so pls help me.
Here is a screencut of the battery information from battery management studio: