This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713EVM-017: Do I need the EV2400 USB adapter to configure?

Part Number: BQ25713EVM-017
Other Parts Discussed in Thread: BQ25713

Hello. I did not understand that we also need the USB adapter and did not order it with the Eval kit.

After looking at the data sheet, my question is: with the eval kit can I just manually write all the configuration registers using the I2C pins with an Arduino or another microcontroller? If it can be configured then I can also read the data back that I need from I2C to make sure the device is working properly. Does this make sense?

I am planning to do this, but I want to make sure there is a chance of success before I spend the time on it. 

Thanks.