This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SLUA962



Messrs TI,

following your application note SLUA962, in order to avoid to damaging the converter because of reverse current, is it possible to choice a synchronous DC/DC converter with a Vin_min>Vout?

If this works the user could avoid to use a UVLO setting with a voltage divider.

  • Hi Dtluigi,

    It maybe work but it's not easy to pick out a part with Vin_min > Vout to meet high output cases.

    BRs,

    Ryan

  • I agree with you, in fact I am focused on low output voltage (3,3V-3,8V).

    Do you think it could be an issue to have a synchronous DC/DC without UVLO divider resistor and with a Vin_min=3V so with a dV=Vout-Vin_min<1V?

    Do you have measured a threshold (Vout-Vin_min) above which it is recommended to use a UVLO divider resistor?

    Regards

    Luigi

  • Hi Luigi,

    Since the output voltage is not very high, it would not be a damage risk by reverse current.

    In most applications, no big reverse current existed. And having reverse current doesn't mean damage risk. Usually we can set the start / stop VIN voltage higher than target output voltage to avoid reverse current damage risk. It's not a must. I have no certain answer if a UVLO resistor network needed. Different Rdson, inductor DCR/Value, different voltage gap between VIN_UVLO and Vout would result in different reverse current. So the answer is case by case.

    BRs,

    Ryan