Hi,
I have some questions about EM1402EVM.
1) In the EM1402EVM datasheet shows an image were the external power supply is 12V/24V but then it says that the positive external isolated balance source input is 12V. What is the correct value or is a range of values between 12V and 14V? What happend if the external power supply is less than 12V? The device turn off immediately?
2) Can the EM1402 EVM performs a balance (charge or discharge of one cell) when the Battery Module is being externally charged? Is there is any risk?
Thanks.