Other Parts Discussed in Thread: BQ2057, BQ24004
Hi team.
I'd like to tell me about Bq2057 operation.
Our customer designed according to the recommended circuit in the data sheet(p.10).
However, the charging operation does not work.
As a phenomenon, the voltage at the CC pin gradually increases and then becomes the same as the input voltage(VCC/SNS).
But the charging voltage is not fully charged.And then
A large current flows through to the load when the CC pin voltage is the same as VCC.
Please tell me about bellow questions?
1. Is it correct which The voltage at CC pin gradually increases
*The increase time is about 5 seconds.
2. Do you have any idea where the problem is that over current flows when the CC pin voltage is the same as VCC?
Sincerely.
Kengo.