Other Parts Discussed in Thread: TPS65251
I think that TPS65251 want to use external synchronization.
TPS65251Datasheet ROSC mention is that If external synchronization is used resistor should be fitted and set to ~70% of external clock frequency.
Internal clock frequency is less than 70% of external clock frequency?
Will it be to say that 70% are good at 0% as follows?
I theoretically think that consistency does not match.
Regard.
Bob Lee