Hi Sir,
Can TPS65262 two - way LDO be used in parallel?
What should I pay attention to when using parallel?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the 2 LDOs are used in parallel, when add loading, they will work in below way:
one of LDOs will not provide any loading, (Marked as 1st LDO)
the other LDO will provide whole loading until reach it's OC limit (Marked as 2nd LDO), then Vout will drop a little, and the 1st LDO will start to provide loading to keep Vout, when both LDO reach OC limit, output will shut down.
So I said "cannot assure the equaled current flowing in 2 LDOs", this is not good working behavior, so I think they cannot be used in parallel.