This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920EVM: BQstudio cannot find the correct device.

Part Number: BQ76920EVM
Other Parts Discussed in Thread: BQSTUDIO, , BQ78350-R1

The BQ76920EVM is running firmware v1.04. When I start the BQstudio v1.3.93, it says that the auto detected device is 1e9b_1_04 then when I choose 1E9B_1_03_bq78350-R1.bqz from the list, it complains that the detected device is not compatible and the system may enter an unrecoverable state. I also tried with the BQstudio1.3.86.3. The result is the same.

How can I proceed safely ?

Thanks in advance.