Hi,
I have a customer that is looking to use the TPS27S100B and we want to make sure that R_imon is set correctly.
They want to use R_ilm as a backup, so they have it set to 510 ohms which should correlate to ~4.8A.
They want to monitor the current via a 3.3V ADC and turn off the output via the enable pin if the current exceeds 4.5A
Equation [1] in the datasheet shows the R_imon = (V_imon * k_imon) / I_out ... since k_imon is set to 500, setting V_imon to 3.3 V and I_out to 5A (to give some margin) provides a value of 330 ohms for R_imon. Does that seem correct or is there something that I am missing?
Thanks
-Tyler