there is an interesting issue when I was test the PSRR. As we know, it is better for us to remove the input cap, the input caps of TPS7A8400 are removed. If connect the board directly to the power supply, there is about 26kHz reponse on Vin which cause large votlage spike on input, when the load is higher than 0.6A, output voltage drops. could anyone tell me how to remove this spile without adding any cap or filter that affects the injuected signal.