Dear ALL
Pls help to suggestion , customer is need to know LM5176 can used for this project yes or not ?
Detail of project is below .
- Input: 17 to 29Vdc (from deep discharge cut off to fully charge 12V*2 SLA battery)
- Output: 24V/19A
- Efficiency: > 91% from 25-100% load
Then i need to know to improved Efficiency at 25% ,50% and 75% Load
The Ref design of LM5176 design of maximum power 300W if you have ref design for project information Pls send to me , i can send to customer .
Thank you so much & Bestregard
Prarinya