I am interested in finding out about the accuracy of the 2.5V and 3.1 V references inside the UC2625 motor control chip. The block diagram of the chip shows that there is a 2X gain amplified, an absolute value block, a 2.5 V and 3.1 V reference voltages. The "current amp" section of the data sheet (sheet 4) states that the accuracy of 2x gain amplifier, abs value block and reference voltages all together add up to 30%, which is very high. I would like to use an external gain amplifier but have to rely on internal voltage references, in which case I need to know the accuracy of 2.5 V and 3.1 V reference voltages. I dont expect the accuracy of the reference voltages being that high, but I need to know this in advance.
Thank you,
Muhammet