This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: bq40z80

Expert 1215 points
Part Number: BQ40Z80

Hello,

I'd like to ask what kind of parameters should I adjust in order to get max capacity from the battery.

Let's say I've got:

https://lygte-info.dk/review/batteries2012/Sony%20US18650VTC6%203000mAh%20(Green)%20UK.html

Can I for example set Term Voltage to 2V*6=12V or rather to keep safe margin 2.5V*6=15V?

Regards,

Adam