Hi
Battery 16.8 V, 12 Ah, set 3A charging current, quick charge safety time is set to 5 H (C = 56 nf).
Pre-charge current and terminate current is set to 300 mA but only can be charged to 16.4 V.
Remove the battery test BQ24616 output voltage is 16.8V. After parameter adjustment, quick charge safety time is set to 10 H (C = 0, 1 uF).
The cut-off current is 30 mA, battery only charged to 16.4 V, the final phase is the constant voltage of 16.8 V, why the voltage is 16.4 V,Unplug the battery and test BQ24616 output voltage is 16.8V.
Please give some suggestions.
Thanks
Star