This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: BQ24610 NTC Equation for RT2 and RT1 Help!

Part Number: BQ24610


Hello,

I am having an issue about the equation and how what should be inputted for the following:

Vvref: I have put 3.3 for vref is 3.3V

RTHcold: I have put the resistance value from datasheet of 103AT of 0 degrees which is 27.28k ohms

RTHhot: I have put the resistance value from datasheet of 103AT of 45 degrees which is 4.911k ohms

VLTF: I have put the percentage which is 73.5% from BQ24610 datasheet which is cold temperature rising threshold 

VTCO: I have put the percentage which is 34.4% from BQ24610 datasheet which is cut-off temperature rising threshold 

I have taken a screenshot of the formula I rewrote on to MathCAD

The result for RT2 and RT1 looks very off from what is given as recommended RT2 and RT1?

Please, could I have help on what values I should have put in?

Best regards

Mo