Other Parts Discussed in Thread: BQSTUDIO
Hello! While at rest, the current values of cells 1-4 (in BQStudio) change in time and can take values from -200 mV to + 200 mV. With what it can be connected?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mihon,
Are you carrying out this test on bqstudio or your board? If an evm, run current calibration. If your board, can you check to make sure there isn't a short somewhere that is causing the current drain? Also, try performing current calibration as well
thanks
Onyx
I use my board. Thanks for the tip, I will inspect the board for short circuits. Please tell me, maybe this is due to the fact that I do not use the indication and the corresponding microcircuit pins (20, 21 and 22) are hanging in the air? And can this be due to the fact that I have capacitors C19 and C20 marked DNP in the current shunt circuit?
Tell me, please, is there any minimum voltage value on the cells below which it is not recommended to perform current calibration?
And yet - by what principle is the current calculated through each cell calculated and does the current shunt circuit affect this?