Hi,
My customer is in need of support. please read below:
"I'm currently working on a LCD Display power supply, using TI's TPS65150 chip to produce 4 voltages from a source voltage of +2.5V. I had a prototype PCB made and the circuit mostly functions, except the VGH voltage won't get up to +22V where I need it. I can only reach +16V. I tried adding another charge pump stage as suggested on pg17 of the spec sheet but that just resulted in an unstable output that eventually led to the chip going into shutdown mode. I attached the spec sheet I'm using and the specific design I've worked up. Think you can provide any clarity on this?"
Thanks,
Kevin