This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54308: About ESR of output capacitor.

Part Number: TPS54308

 Hello guys,

 One of my customers is designing their own PCB to evaluate TPS54308 for their new products.

 They have the following questions about output capacitor ESR. Could you please give me your reply?

 Q1. ESR can be calculated by equation 13 on page 17 in TPS54308 datasheet(SLUSCV2).

       Also capacitor ESR is changed much by frequency. (For example, 10ohm (at 0.1Hz) ~ 3mohm (at 1MHz)

       Which ESR frequency  should be compared with the valure calculated by the equation?

       Is it the switching frequency of TPS54308?

 Your reply would much appreciated.

 Best regards,

 Kazuya.