This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Switching regulator that covers wide range of output current with high efficiency

Other Parts Discussed in Thread: TPS63805, TPS63802, TPS63000

Hi,

Requirement:

Vin: 3 to 4.35V

Vout: any voltage between 1.8V to 4V

Iout: 1uA to 700mA

I have 3 loads that draw current as low as 1uA (standby/sleep mode) and as high as 700mA (peak/active mode).

I need switching regulators that have high efficiency at very low current 1 uA and peak current at 700mA of the loads. If there is, can you suggest me some part numbers?

Efficiency: 80% to 95% if possible. Any suggestion or advice is welcome.

Thanks.