Other Parts Discussed in Thread: UCC2800, UC3842A, UC3842
Hi HVC team,
Question above. The max duty cycle is 100%, is it possible to limit to 80% (for example)?
Thanks,
Lauren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi HVC team,
Question above. The max duty cycle is 100%, is it possible to limit to 80% (for example)?
Thanks,
Lauren
Is there an update?
Thanks,
Lauren
Hi Lauren,
Sorry for the delay.
Refer figure 5 and figure 9 in the datasheet, We can limit the maximum duty cycle by regulating the dead time. But it can only realize a very small range regulation. I don't think there in a good solution to limit maximum duty cycle for UCC2800.
The duty cycle of UCC2800 cannot be easily modified by adjusting RT and CT, unlike the UC3842A family. The maximum duty cycle limit is set by the ratio of the external oscillator charging resistor RT and the internal oscillator discharge transistor on-resistance, like the UC3842. However, maximum duty cycle limits less than 90% (for the UCCx802 and UCCx803) and less than 45% (for the UCCx804 and UCCx805) can not reliably be set in this manner. For better control of maximum duty cycle, consider using the UCCx807.
Regards,
Teng