I am working with LMR14020, it has internal two mosfet, high side and low side.
If the low side mosfet becomes open circuited,then how will the regulator will behave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am working with LMR14020, it has internal two mosfet, high side and low side.
If the low side mosfet becomes open circuited,then how will the regulator will behave
Hi
LMR14020 is asynchronous DCDC converter, the low side is only used for charge the boot cap, it will only turn on for a very short time. if low side mosfet is open, it will not affect the conerter in normal operation. but if the converter work at no load condtion, the boot capacitor will not be charge enough , make the high side mosfet keep turn off.
thanks
Daniel Li