This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A-Q1: Top rail getting hot

Part Number: BQ76PL455A-Q1
Other Parts Discussed in Thread: BQ76PL455A

I just made my own BMS using the BQ76PL455A following the eval board for the most part. Upon first testing I noticed that the two 200ohm resistors that are on the top line get really hot, like excessively hot. I was wondering if anyone else has come across this or why this would be happening? Also why is the design recommendation to put two 200ohm in series instead of just one 400ohm? Any answers would be appreciated, thanks.